This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ads1298 wct配置问题

Other Parts Discussed in Thread: ADS1298

你好,

我采用ads1298,模拟器输出ecg数据,WCT配置如下:WCT1 = 0x09,WCT2=0xD5,将与 ch1 N、ch2 P、ch3 N三个通道相连的RA、LL、LA选中作为三个放大器的输入,WCT引脚电路中连接的是ch4~ch8的N端,现在的现象是胸导联有较大的噪声成分,经过matlab分析发现50hz成分偏多。我的调试过程如下:

1、关闭三个放大器, 胸导联的基线漂移至0x7fffff附近,噪声成分还是较多,说明之前的配置,放大器是在工作的;

2、打开三个放大器,同时设置WCT1=0xF9,WCT2=0xD5,即打开加压肢体导联的4个bit,发现噪声成分显著减少,可以看见ECG波形,但是各个胸导联的波形形态发生了畸变,S波峰被放大了。

WCT外接的电容我从51pf,100pF,1nF都试过了,没有解决问题。

另外,肢体导联I、II、III的波形都是正常的。

请问各位,这是什么原因导致的