Other Parts Discussed in Thread: TUSB8020B, TUSB4020BI
现在设计一个产品,需要两个USB接口(一个USB TYPE A,一个USB TYPE C)和一个SD卡接口。两个USB接口需要支持充电和传输信号,并需要支持carplay。TI是否有满足要求的方案,请推荐。carplay 的功能需要upstream支持OTG(device和host)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TUSB8020B, TUSB4020BI
现在设计一个产品,需要两个USB接口(一个USB TYPE A,一个USB TYPE C)和一个SD卡接口。两个USB接口需要支持充电和传输信号,并需要支持carplay。TI是否有满足要求的方案,请推荐。carplay 的功能需要upstream支持OTG(device和host)
TUSB4020BI 是USB2.0的HUB,并且支持DCP,CDP充电模式,但HUB upstream是不支持OTG功能的。 在datasheet中有典型应用,上行端口接的是host,下行端口接的都是device:In this application using a USB cable, TUSB4020BI device’s upstream port is plugged into a USB host controller. The downstream ports of the TUSB4020BI are exposed to users for connecting USB hard drives, camera, flash drive, and so forth
最好有整体方案,可以不是单独的一颗芯片实现功能,可以用其他单独的芯片组成一个满足要求的方案。谢谢!