This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

drv8353rh_evm开发板 3.3VLDO发热问题



板卡上的稳压管 型号 LP2992IM5-3.3/NOPB,12V的输入  提供3.3V输出,250mA的固定输出,插上 控制板卡ISO-F28027F 发热现象严重 ,(没有测温设备)手无法长时间触碰的情况,拔掉控制板ISO-F28027F给驱动板单独上电,是24V 3mA的功耗 ;   控制板卡ISO-F28027F单独上电是 3.3V  58mA的功耗; 相当于200mA的电流发热耗掉了,这个现象正常吗,长时间使用会有问题吗?