This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

咨询高精度ADC芯片

Other Parts Discussed in Thread: ADS1246

您好!

        我这边有测距传感器应用,输出的是模拟电流信号4-20mA,对应测j距范围为10-130mm,要求测量精度为0.1mm.我需要对此芯片进行ADC采用。希望采用下图方式由电流转换成电压进行采用,下图是差分输入的,实际是需要单端输入。如果采用参考电压4.096V,采样电阻为200Ω情况下,采样精度至少要1mV才能满足应用,最好是0.1mV,采样频率至少1K,希望可以2K这样,麻烦推荐几款性价比高的芯片,通信接口可以SPI,I2C,谢谢!