This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC161S997使用问题



这个4-20mA输出的DAC芯片,我有按官方的方式连接,但是LDO始终输出不了3.3V,所以芯片没能正常工作,LDO的地是和DAC共地的,请问可能的原因是什么?

方便微信回复吗?15000256530

  • 您好,您参考下datasheet Page25介绍,如果想得到稳定3.3V LDO输出,需要满足下面条件:www.ti.com/.../dac161s997.pdf
    To ensure stable 3.3-V LDO output under these conditions, the following relation must be fulfilled.
    V(IN_LDO) (at minimum VSUPPLY & minimum ILOOP ) > VIN_LDO (MIN REQUIRED at 3.3 mA) (17)
    [(100 Ω × 200 μA)+ VZENER + 0 V + (20 Ω X 200 μA)] > 3.4 V
    [VZENER + 0.024 V] > 3.4 V