This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1220问题请教

Other Parts Discussed in Thread: ADS1220

尊敬的TI专家:
 
      您好,我们准备用ADS1220搭建热电偶采集电路,初步构想如下:采用8片 ADS1220,每片ADS1220的CS管脚对地,CLK、SCLK、DIN
共用,每片ADS1220的DOUT/DRDY管脚单独引出, DRDY管脚引出一个即可(判断数据准备好信号),这种方案是否可行,谢谢。
      另,在冷端补偿时,无论是芯片自带的测温采集,还是外接RTD测温,在正常采集热电偶信号时,间隔多长时间采集冷端补偿信号比较好,
谢谢。
  • ADS 1220 不支持菊花链的级联, 但可以共用SPI 端的SCLK, DIN, DOUT, 片选CS需要单独控制,以便每次只能对一片ADS1220进行通讯.
    同时data ready available功能也不能使用DOUT/DRDY 引脚了,只能使用DRDY引脚.
  • 楼主的这个连接应该不是属于菊花链的连接,我的理解是,由于有/DRDY管脚的存在,是可行的。但是你的/DRDY管脚需要使用专门的引脚,不能和DOUT引脚混用,你每个芯片需要单独的把/DRDY和DOUT管家接出来,数据手册也间接说出了这种方法是可行的。