This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38J82输出不正常



问题1:

配置:LMFK=1:1:2:32  1DAC,不插值(250Mfs linerate=5G);

问题现象:循环输出从0x1000~0xF000累加的锯齿波形,波形上叠加有高频杂波,可能是什么导致的?如何去除这种杂波。

问题2::

配置:将上面的采样率提高到2G(其它参数不变),插值为16,2DAC(2G/16/2DAC=250M,同上);

问题现象:无任何波形输出;插值需要特别注意什么参数吗、例如插值滤波器设置?

问题3:如果用2个DAC,FPGA的M也需要设置为2吗,FPGA GTX的tx_aresetn时高时低,无法正常工作。