This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4017BPWR使用?



一、故障现象:

  1. 故障产品通遮光状态下输出信号正常转换,但受光器红色指示灯偶尔闪烁;
  2. 测量各信号,发现RST信号偶有缺失;测试发现为CD4017 Q3信号不正常。
  3. 将受光主板RST跳线(JP1)更改至Q4位置,光栅工作正常,受光器指示灯正常,测量RST信号正常;
  4. 更换U3(CD4017),光栅工作正常,受光器指示灯正常,测量RST信号正常。麻烦帮忙看下是否为CD4017的问题?

  1. 根据4017的器件资料,其电源电压10V下状态为0的输入电压典型值为4.5V,4050的电源电压10V下状态为1的输出电流典型值为2.6mA,因电路中22K电阻限制,其充电平均电流达到0.443mA,根据Q=CU=It,可以计算得出从0V充电至4.5V的时间为10.15us;
  2. 器件4017的信号上升沿和下降沿均为ns级别,见图2,电源电压10V时时间小于500ns,器件4050的信号上升沿和下降沿也为ns级别,见图3,电源电压10V时时间小于80ns,所以经过延时后RST信号可达到10us左右;

图2,4017上升沿和下降沿参数

图3,4050上升沿和下降沿参数