大家好,现在我是用ADS1274这款芯片,配置的是低速SPI固定位置输出模式,从DOUT1引脚接收数据,每个通道取前16位的值输出,现在我的VREFN接地,VREFP接2.5V参考电压,现在AINP1,AINN1,AINP,3,AINN3,AINP4,AINN4都是接的2.5V参考电压,AINP2和AINN2分别接的是0.9V和0.7V电压,但现在采集的数据显示通道一,通道三和通道四都是0X8000,通道二则是0X7FFF,理论上来说差分输入通道一,三,四不会是8000,通道二也不会是7FFF吧,毕竟AINP-AINN没有达到正负最大量程,不知道现在是什么原因,输入电压改变也还是不行,求解答。