你好,我是一个新手,想请教一下,我们有块STM32的MCU,但是上面的ADC不能多通道同时采样,所以初步选了ADS8568。但是看了芯片手册之后,有些疑问:
1.ADS8568支持并口和串口,因为不熟悉并口读数,里边的串口支持四通道输出,但看起来和QSPI的数据格式对应不上啊:ADC每通道的采样数据通过一个输出通道输出,而QSPI的4根数据线的数据是相关的,所以应该如何读取呢?
2.ADC没有缓存,这样我就需要每次采样完成之后我的MCU就需要读一下数据,,如此一来,500K的采样频率就需要2us读一次数据,,这样MCU就没有其他时间做其他事情了呐,应该如何解决呢?
目前,我手上的STM32 MCU上就是有个FMC和QSPI等接口,,应该如何使用这个ADS8568呢