A single ground plane is recommended for the AD9814. A separate power supply may be used for DRVDD, the digital driver supply, but this supply pin should still be
decoupled to the same ground plane as the rest of the AD9814.
AD9814手册有这样一段,关于地平面分割的。PCB上其他地采用AGND和DGND分割的策略,如果操作AD9814呢?以下有几种理解,哪个正确呢?
1. single解释为“单独的”,AD9814需要一个单独的地平面,即除了AGND和DGND,还需要一个AD_GND。那这个AD_GND如何与AGND和DGND连接?分别单点接地吗?
2. single理解为“同一个”,强调AD9814下面不分地,其他区域的AGND和DGND在AD9814下面强连到一起,整个PCB等同于只有一个GND,只是其他位置有槽分开,AD9814是完整的铜皮GND。
3. 最后一种就是忽略这段话,在AD9814下面根据模拟和数字管脚,将芯片人为的分为AGND和DGND,在芯片的bottom层或者远端加一个0欧电阻单点接地.
哪种分地更合理呢?上面那段话的single强调的是“同一个”还是“单独的”呢?有些ADC手册不提分地(circuit and layout),管脚有模拟地和数字地的区别,这时应该如何分呢?
非常感谢!