Other Parts Discussed in Thread: ADS1274, ADS1294
1、ADS1274和ADS1294有什么区别吗?如果我想选一个四通道的24位数据采集系统,采集对象的模拟前端为运放的输出,选哪一个好,ADS1294是不是只用于ECG和EEG呢?
2、ADS1274的datasheet显示他的SNR为111dB,是不是说他最高只能达到这么大,因为我看到他的时钟fCLK/fDATA数据输出固定一比值,那么我如果想通过降低数据输出速率(采集信号带宽为50Hz,不需要这么高的数据率数据)的方式提高SNR的话,是否只有在控制器里面通过数据平均的方式来实现。
3、在ADS1274里,我如果通过降低时钟频率fCLK的方式来降低数据输出速率,是否不能达到降低SNR的效果?此外,在ADC中,在信号带宽不变的前提下(数据输出率不变),如果提高采样率,SNR肯定增加吧。