我在阅读TSW1400evm的userguide时 在software start up这一块,从TI官网上下载的tools压缩包,解压后并没有userguide里面所说的那些文件夹( Under this folder will be a “setup.bat" file, a folder called “EVM GUI” and another folder called “FTDI”. The EVM GUI folder contains the GUI code and the other folder contains the drivers for the USB interface.)
但是,解压slwc107d这个文件夹只有:High Speed Data Converter Pro - Installer v2.0这个应用程序,没有所说的 “setup.bat" file, a folder called “EVM GUI” and another folder called “FTDI”. The EVM GUI folder contains the GUI code and the other folder