This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVCH8T245 ESD标准及电流功耗评估问题

Other Parts Discussed in Thread: SN74AVCH8T245

Hi ALL

1:SN74AVCH8T245 的ESD标准从Datasheet 7.2节可以查到其HBM标准为+-8KV,比之前的 hc244或者HC245等芯片2kV的ESD标准高很多,这是此芯片特有特性吗?如果此芯片用于JTAG,有推荐的TI ESD器件吗?

2:SN74AVCH8T245 的pin 2引脚DIR Datasheet要求其上拉至VCCA,其上拉电阻取值是多少?可以直接通过0R上拉吗?

3:SN74AVCH8T245 工作在VCCA=3.3V VCCB=1.5V 数据速率30Mbps 8端口同时使用,方向固定由A到B,其静态和动态的总工作电流或者功耗是多少?我们需求根据此参数评估电源树设计。  确定 sn74avch8t245.pdf 

  • 您好,

    1.您这里需要推荐ESD器件,是需要IO口再加上ESD保护器件吗? SN74AVCH8T245的ESD防护等级 如果够用的话,可以不用再加ESD器件。

    2. 可直接上拉。

    3)静态工作电流可直接参考datasheet中的Table 1. Typical Total Static Power Consumption (ICCA + ICCB)

    动态电流的话, 根据实际应用接的负载情况,可实际测量下。