This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于INA190A1测电流



最近设计中用到INA190A1这个片子来测电流,电路是datasheet中的标准电路,INA190A1的供电是3.3V,采样电子是1Ω,对mA级(10mA-100mA)的电流进行测量,但是测出来的结果总是要比实际值大5mA左右(比如实际是40mA,但是芯片测出来的却是45mA),已经排除采样电阻精度不够,这颗芯片不应该有这么大的误差吧?请问会是哪里的问题吗?

  • 您好,可能是由于Rsense阻值太小,在选择Rsense的时候,太小了会影响精度,太大了会产生Gain error,所以datasheet中给出了Rsense的取值公式,Voutmin=Imin*Rsense*Gain。 可根据自己实际需求,计算下Rsense的值,建议Rsense小于1Kohm,如果在计算过程中,Rsense超过了最大值1K,那么就选择1Kohm阻值。