Other Parts Discussed in Thread: TDP142, TDP158, LMH0341, DS32EV400, TVB1440, DS32EL0124, DS32ELX0124
请教下,TDP142是否可以用于类似高速数字信号SDI的6GHz信号传输,补偿长距离传输产生的损耗问题
如果可以,有无使用限制,目前来看TDP158时钟通道是不可以的,TDP142则没有任何限制,是这样的吗?
感谢回复!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TDP142, TDP158, LMH0341, DS32EV400, TVB1440, DS32EL0124, DS32ELX0124
请教下,TDP142是否可以用于类似高速数字信号SDI的6GHz信号传输,补偿长距离传输产生的损耗问题
如果可以,有无使用限制,目前来看TDP158时钟通道是不可以的,TDP142则没有任何限制,是这样的吗?
感谢回复!
Hi kailyn,serdes是Xilinx 的一种高速数据接口,全称Serializer-Deserializer,是一个串并行转换的模块,我们的产品就是两个FPGA远距离传输6Gbps的serdes串行数据,有四路6Gbps信号,所以找到了这两个芯片,还请确认下
Hi kailyn
我们是xilinx显示类的FPGA,应该是类似VDS的数据类型
这么说吧,以前旧的3Gbps平台用过DS32EV400和TVB1440,是没问题的