This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC1080(温湿度传感器)的湿度测量非常不准确,尤其是在高湿度的情况下

Other Parts Discussed in Thread: HDC1080

(1)HDC1080温湿度传感器芯片,当环境湿度在80%左右的时候,HDC1080检测到的湿度在90%以上。而且芯片周围并没有自发热的影响。

(2)同一批次的HDC1080自身之间的一致性都比较好,也就是说,大家都一起Offset了10%以上。

(3)温度检测都比较准确。

(4)我们采购的不同批次的芯片,它们之间的湿度Offset的大致平均值还不一样,有的漂得远,有的好一些。

(5)SMT贴片是严格按照datasheet要求的。而且,我们也手工焊接了一些样品来测试,结果一样。

(6)我们两年前项目刚开始的时候采购的少量HDC1080很准确,都通过了上海计量局的检测的。

HDC1080的这种表现,简直就没办法用啊!使我们哪里搞得不对?

我们采购的也是正规渠道,从“立创商城”采购的。

  • 补充一下,上述测试是在环境温度约25℃的情况之下。
  • 您好,湿度温漂的影响主要和芯片存放周期时间长,从而受到空气中的灰尘,汽化溶剂,粘合剂等影响,在datasheet中也有描述:

    Drift due to aging effects at typical conditions (30°C and 20% to 50% RH). This value may be impacted by dust, vaporized solvents, outgassing tapes, adhesives, packaging materials, etc.

    另外,推荐的湿度操作范围在10% to 70% RH范围内,超过这个范围就很有由于offset的影响导致测量不精准。

    )Recommended humidity operating range is 10% to 70% RH.

  • 通过HDC1080上的丝印mark,能查到芯片的出厂日期吗?丝印为781R字样。
    是在是偏差太大了,简直不能用。
    而其他厂家的SHT20没发现有这个问题。
  • 您好,很抱歉,依据相关政策,已经不再提供通过丝印查询出厂日期的服务,但是可以通过下面这个链接查询具体芯片的丝印是什么, 比如HDC1080的丝印应该是1R。www.ti.com/.../partlookup.tsp

    您是通过TIestore购买的吗?