我们通过TUSB1046想做DP信号切换,使TypeC能输出DP信号,typec通过CC协商已经进入alt mode;
tusb1046使用的i2c模式配置,根据datasheet 寄存器0x0a的 CTLSEL1 CTLSEL0 FLIPSEL 配置lane和aux->sbu,
平台端报aux 读写错误,请问tusb1046做DP切换,通路配置有什么需要注意的?
期待回复
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,Table4 指的是输入输出接口的路由,适用于GPIO和I2C mode。
但是AUXp / AUXn 到 SBU1 / SBU2的路由在I2C mode下需要参考Table 6.
I2C mode下,CTL0与FPLIP 上拉到VCC即可。