This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Q1:用软件连接设置dac81416的每个通道的电压值之后,怎样可以断开usb2any之后,dac81416每个通道还能输出之前设置的值。
Q2:可以不通过pc使用usb2any连接dac81416吗,可以使用外部信号单独连接到miso、cs、sck等引脚上进行dac配置吗?
Q3:我是用fpga连接到dac81416上,时序满足dac的要求,电源供电也设置的符合要求,但是dac通道输出都是0,请问可能存在什么问题。
请问只能用pc控制dac81416吗?可以通过其他方法比如fpga来驱动dac吗?
我是通过fpga和DAC81416直接通讯的,fpga提供了CS、SCLK、SDI信号且符合81416技术手册21页上的图45提供的时序(如上图所示),并且供电VIO、VSS、VCC、VAA/VDD。信号是通过杜邦线由fpga接到usb2any所对应的引脚上的。下图为FPGA生成的spi信号,sclk信号接到DAC的J8.8,CS接到J8.2,Sdout信号接到J8.4,J8.5接电源,J8.6接地。但是DAC输出电压全部为0,我设置的并不是0。请问我这么做,可能存在什么问题导致DAC不能正常工作。