Other Parts Discussed in Thread: ADS7229
用CPLD控制ADS7229,因为需要用到状态机,需要了解7229的工作流程是怎么样的,手册上没有看懂,望大侠指点!
比如:流程一:通过SPI接口进行寄存器(CFR)配置——》启动转换-——》等待转换完成——》输出数据(sdo)——》启动下一次转换?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS7229
用CPLD控制ADS7229,因为需要用到状态机,需要了解7229的工作流程是怎么样的,手册上没有看懂,望大侠指点!
比如:流程一:通过SPI接口进行寄存器(CFR)配置——》启动转换-——》等待转换完成——》输出数据(sdo)——》启动下一次转换?
你好,我现在ADS7229可以正常采到数据了,但遇到另外一个问题,就是经常上电芯片起不来,芯片一直没有EOC信号输出。
我采用的模式为自动触发,配置参数为:1110_1101_1111_1101,这个D4位应该配置成1还是0呢?有个奇怪的现象,就是上电后
如果芯片没起来,我拿示器探头点一下芯片Pin11脚(CS),会诱发芯片正常工作,但即使这样,工作一段时间也会出现芯片停止
工作。ADS7229我是用FPGA控制的,控制流程里如果一直检测不到EOC信号,会复位芯片(1110_1101_1111_1100)然后再配置
芯片(1110_1101_1111_1101)。以上请答复,谢谢!