您好!
我现在遇到一个问题,信号板上面的ADS1255开机不到1分钟就发烫,我不知道是什么原因,可能是我原理图有问题也可能是PCB布局的问题,现在我把原理图贴上,还请帮我一起查下原因,谢谢了啊。AVDD是模拟5V,VREF是2.5V,稳压管是4.7V的,数字电源是3.3V,还有5路与CPU通讯的。连接CPU后读取ID很多为00,正常的板子是30.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
我现在遇到一个问题,信号板上面的ADS1255开机不到1分钟就发烫,我不知道是什么原因,可能是我原理图有问题也可能是PCB布局的问题,现在我把原理图贴上,还请帮我一起查下原因,谢谢了啊。AVDD是模拟5V,VREF是2.5V,稳压管是4.7V的,数字电源是3.3V,还有5路与CPU通讯的。连接CPU后读取ID很多为00,正常的板子是30.

我将电感换成0欧姆的电阻试过,也是发烫的。
发烫时,输入信号AIN0为0.29V,AIN1为0.145V。 就算我将R306 R309去掉也是发烫的。同时我也测量了VREFP的2.5V,VREFN是0.03V。
我将D0引脚悬空试了下,通电一会还是发烫。
寄存器和PGA是软件工程师配置的,这个发烫的现象跟软件有关系吗?我问了PGA配置的是1倍。寄存器设置的是0.