This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

项目需要将MCU输出的信号转成4mA-20mA输出,电路需要工作在-55℃~70℃,求各位大神出出方案

Other Parts Discussed in Thread: DAC8760, XTR111

我想到几个方案,大家帮忙评估一下:

1、MCU + 电流型DAC,MCU通过数字接口(IIC等)与电流型DAC通信,控制DAC输出电流,最好是双路输出DAC。

2、MCU+电压型DAC(最好双路输出)+ V/I电路

器件需要在-55℃~70℃工作,大家帮忙推荐一下方案、电路以及器件,感谢!