This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC6140采样率的合理设定



目标,设置采样率16kHz,16bit

当前配置:

1.Mclk外接入12MHz,

2.0x13寄存器配0x80:bit3 FS_MODE是什么意思,是ADC以48kHz采样?还是I2S以48kHz传输?怎么用16kHz

3.0x14寄存器配0x14:

输出来的数据采样频率为60几,不是16k?

请问如何配16kHz采样率?

  • FS_mode指的是当ADC6140工作在master mode时候,ADC采样率的设定,当FS_mode=0时,fs为48Khz的倍数(或约数)。当FS_mode=1时,fs为44.1Khz的倍数(或约数)。可以看下Table 6 和Table 7 分别在FS_mode=0 和1 时FSYNC和BCLK的频率。 

    您是需要16Khz的输出是吗?