This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1220IPWR相关问题咨询



以下3个问题可否帮忙确认下,谢谢!

1、请问EXC1-接电阻桥负激励端,芯片内部这个脚是不是接地?

2、独立的两路AI1和AI2与差分信号的参考电压是可以分开还是需一致?混合使用时,基准参考电压是怎么分配的?

3、电阻桥模式时的配置有参考吗?

每个数组三个参数第一个和第二个分别是独立的4-20mA电流AI信号,第三个参数是测差分信号的,如附件截图

  • 1. REFN0是参考输入的负端输入,内部并未接地,它的输入电压范围为AVSS-0.1V~V(REFPx) – 0.75V 这个范围。
    2.AIN1 ,AIN2 是和AIN0和AIN3都一样的,只是AIN0和AIN3还可以作为参考输入。
    这几路输入是需要经过前端MUX 之后选择哪一路进行导通,参考register0的 MUX[3:0]的配置。所以不能混合使用。
    3. 很抱歉,没有参考配置可以参考。