This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1258的问题

Other Parts Discussed in Thread: ADS1258

专家们好:请问下ADS1258在外接32.768K的晶振时,晶振到管脚的距离限制最大是多少啊?我现在在用ADS1258的测试的时候发现芯片好像没有工作,电源部分和焊接我都测试过了没有问题,请问会是什么原因呢???

  • 关于晶振和内部PLL的连接请参照datasheet上的连接图。

    先用示波器检查一下32.768K晶振的引脚,看一下有没有起振。

  • 需要尽量靠近,请测量晶振是否起振,摆幅多少?

  • 专家,请问下,在ADS1258的单向AIN端的输入很小很小的时候,比如只有10mv左右的话,这个ADS1258能正常转化出来吗?我现在接的单向输入很小的时候,AD转化以后得到的数值很大很大,在datasheet上没看到说关于输入很小的时候输出会怎样的描述,向专家咨询一下。

  • 我现在用的ADS1258在输入基本为0的时候检测到输出是10.66,AD的输入是接到max4080的输出上,我用万用表测量出max4080的输出为0,万用表量AD的输入端也是也是0,但是转换出来的输出就是上面的那个数,这个数不是用万用表量的,这个输出是通过USB信号传到一块液晶屏上显示出来的,这块AD在检测其他通道的时候是没有问题没有出错,就是在检测max4080输出到AD输入的这个通道的时候就出现上面的情况了,请问专家们这是什么问题呢??

  • 首先10mV的信号对于24bits的ADC来说已经不算小了。小信号时主要受两个方面的影响,一个是offset,一个是噪底,但这两项都在uV级。但对于10mV相对而言是很小的。

    请问你的输入小信号是相对于AVSS的嘛。ADS1258的输入电压范围是不能达到电源轨的,AVSS – 100mV至AVDD + 100mV。

  • 请问你的10.66的单位是V还是code的平均值?

  • 10.66单位是V,是我根据datasheet的公式计算出来的,我的AVSS是接地的,AVDD接的5V。

  • 请问专家到底怎么回事啊?是AD坏了吗?我把电路板的地直接接到AD1258的输入端,读出来的数也不是0,也是10.66V,ADS1258和电路板是共地的,是否会是这个芯片坏了呢?但是在有电压输入的时候,比如输入到AD的电压为2.5V的时候,就能正常转换出来,这是为什么呢?而且我这里有2块一模一样的电路板,一块是好的,完全正常,而另一块就是我上面说的情况。有问题的这块电路板上的ADS1258已经更换过一块新的了,问题还是存在,晶振也换了,求专家指导啊。