This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G125使用问题?

Other Parts Discussed in Thread: SN74LVC1G125

使用SN74LVC1G125时,若采用3.3V供电,其I/O口能接5V的信号吗?

  • 您好,

    若采用3.3V供电,其I/O口不能接5V的信号,从下面文档中可知,SN74LVC1G125输入电路没有至电源的钳位二极管,因此不能接高于供电电压的信号:

  • 您好,SN74LVC1G125在不损坏的前提下,最大输入电压范围为6.5V,是不依赖于VCC的电压,所以3.3V供电,输入是可以接5V的。
    一般在判断Vin是否可以高于Vcc的时候,可以看下datasheet中Absolute maximum ratings这个表格,如果输入电压不能高于Vcc,那么一般最大输入电压范围为Vcc+0.5V ,而可以高于Vcc的器件,最大输入电压是独立的,比如6.5V,不管Vcc电压多少。
    另外,也请参考关于这个问题的FAQ:
    e2e.ti.com/.../723607
  • 抱歉,我对内部钳位二极管的作用理解错了,SN74LVC1G125是可以接5V的信号,但是请注意VIL 参数(Low-level input voltage),在3.3V供电时,最大的低电平是0.8V

    如果有到VCC的钳位二极管,输入高于VCC就会有反向供电。第二,通过钳位二极管的电流有可能变得非常大,从而永久性地损坏设备。