This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps658640配置问题



针对ZYNQ+ULTRASCALE的FPGA供电一些疑问(比如XCZU15EG-FFVB1156I型号):

1:这个芯片的输出配置可以通过I2C接口进行配置,有个疑问,就是板子在SMT贴片回来以后,请问第一次上电,这个I2C接口配置是通过外部进行配置,如果未配置,电源芯片输出会是一种什么状态,是否存在输出电压不对导致FPGA烧毁,另外这个配置进去之后可以掉电保存内部寄存器状态吗?不太清楚这个逻辑。I2C接口可以连接FPGA管脚,同时预留对外I2C接口,如果FPGA没上电,I2C怎么配置PMIC芯片,是否需要外部I2C接口电路进行配置。

2:这个芯片初次上电默认的上电时序是如何的,因为FPGA的上电时序有要求,是否需要初次上电用外部I2C接口进行配置CTL1-6。

3:BUCK1和buck2的电流取决于外部EFT,这个电流是否有最大限制,比如20A等等。