This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DAC60508设定DAC 寄存器,相应的输出端没有电压输出,从芯片里读出设定的值也是正确,但是就是没有电压输出,这是什么原因呢(能够成功设定内部参考使能和不使能,也能够成功设定POWER-DOWN ,但是就是不能输出电压)
可以读出ID:28 16
配置的是异步模式,往DAC2寄存器写入的是 0x80 0x00(打开了内部参考,2.485V,用万用表测出来的)
读出来的也是0X80 0X00
但是DAC2输出的电压是0V,一直是0V,表笔测量的是R117的左端
找到原因了,是因为DAC60508参考默认是2.48V没有进行衰减,设置成1/2衰减就能正常输出了,但是为啥不进行衰减就不能输出呢,即使设置输出电压没超过范围也不能输出