This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1262在±2.5V模拟供电下,可以使用内部2.5V基准吗?

Other Parts Discussed in Thread: ADS1262

ADS1262供电配置为:AVDD接+2.5V,AVSS接-2.5V,DVDD接+3.3V,DGND接地(该地与±2.5V的地在3.3V稳压LDO附近短路)。上电后,没有对ADS1262作任何操作,REFOUT端电压为-0.08V,不是2.5V。请问这样的情况正常吗?之前使用过模拟部分+5V供电的方式,硬件和软件都工作正常。谢谢!