Other Parts Discussed in Thread: ADS1274, ADS1256
根据ads1274的SNR计算该AD能达到的有效位数约为16.8位,不知能否通过降低采样率等手段使得接近24位(不考虑前端处理电路的影响)?请问TI的工程师,你们曾达到的最高有效位是多少?另外,其它24位的AD,有没有做到接近24位的?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADS1274在高分辨率模式下的SNR为111dB。相对应的ENOB为18.14位(最高)。此时采样率为52,734 sps.
由于delta-sigma型ADC的原理,采样速率越高,SNR越差。在分辨率为24bits的ADC中,由于量化噪声的器件噪底的存在,ENOB一般达不到24位的。
如果采用的2.5V的基准,当输入FSR为+/-REF时,一个LSB对应的电压值为0.3uV. 你的系统中果真需要这么高的分辨率?
TI的ADS1256的一款超低噪声的ADC,它的Noise-Free Resolution最高可达23位。非常接近24bits.
ENOB最高可超过24bits. (在最低采样率时)