This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8684IDBTR 芯片故障,请分析下故障原因的定位与分析。谢谢。

Other Parts Discussed in Thread: ADS8684

  • 您好,
    您可以把您的原理图附上来吗
    未去除REFIO和REFCAP管脚电容时,这两个管脚电压均为3.798V吗?去除之后REFIO为3.798V和REFCAP为4.090V吗?
    更换IC后测试REFIO为3.798V时,REFIO pin有接其他负载吗,REFIO和REFCAP管脚电容是极性电容吗,确认极性是否接反?
    异常时测试AVDD等各供电电压正常吗,测量REFIO为3.798V和REFCAP为4.090V时,参考点一样吗
  • 原理图已经附上,麻烦您看一下
  • 您的电路我没看出哪里有问题,但是我有一点比较奇怪,查看ADS8684内部基准电压内部电路(数据手册Figure 57. Device Connections for Using an Internal 4.096-V Reference),REFCAP是REFIO的跟随输出,而您测得的REFIO是3.798V,REFCAP是4.090V,我实在想不出是什么原因会使REFCAP能高于REFIO
    ADS8684采用了SAR ADC结构,由于在每次转换过程中参考电压被采样多次,内部SAR ADC的参考输入引脚向参考源提供动态负载,其中存在电流瞬态,因为在转换过程中内部电容阵列被充电。REFIO引脚需要10uF旁路电容器,REFCAP引脚需要靠近设备的22uF旁路电容器。在转换过程中,旁路电容器是保持参考电压稳定和达到所需分辨率所必需的。旁路电容器被用作电荷库,帮助缓冲器为这些电流瞬变提供瞬时电荷。如果没有所需的REFIO和REFCAP旁路电容器,在执行每次转换时,基准电压可能不稳定和/或在转换过程中下降。
    所以请检查电容的电容值、额定电压及PCB设计是否存在问题,数据手册55-56页提供了PCB板布局建议。此外,下面是一个博客链接,该博客对SAR ADC的旁路电容进行了一般性讨论:
    e2e.ti.com/.../sar-adc-pcb-layout-the-reference-path