前不久TI推出的DAC3484可以对大支持多大的信号带宽?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DAC3488在 1.25 GSPS 速率下比速度最接近的 4 通道 DAC 快 25%,而每通道功耗仅为 250 mW, 比性能最接近的同类竞争产品低 65%。此外,DAC3484 还比其它 4 通道 DAC 解决方案小 40%,并支持高达 250 MHz 的宽带功率放大器线性化。具有更高输入总线的 DAC34H84 或双通道 DAC3482 可支持高达 500 MHz 的线性化带宽。
更多具体信息,请参见: www.ti.com.cn/.../dac3484
Li
也可以关注一下DAC34H84.这个芯片在封装上和3484有所不同,接口速率会降低。性能是一样的。给您多一个选择。