This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC81408适合做信号发生器吗?8路输出,频率40-60Hz,各路相位相对可控,幅度最大10V。



问题如题,欢迎帮忙推荐其它更适合的芯片方案及相关技术文档。精度越高越好!!! 此产品应用于电力设备的内部自校准。

关于精度还有些疑问:除了位数 INL还有哪些参数需要考虑对最终输出精度的影响?

另外,供电电源纹波我们是否需要做精心的控制,来保证精度?

关于精度我们暂定的控制目标:

幅度:1mV

频率:0.001Hz

相位:0.2°