This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12D1600RF对输入1750M到2750M的宽带信号进行采样性能如何?



如题,用上述ADC3.2G采样率,采样1G带宽的信号(1750M到2750M)。

1、我看手册ADC的3dB带宽到2.7G,输入频率到2.7G的话有效位只有7.5位,这7.5位是肯定能达到,还是只是理论值。这样性能是不是不太稳定。

2、我看到手册下方说可以使用3dB带宽以上的频率,但是需要补偿,这个补偿我看AD里没有相应的寄存器设置啊?

求大佬解答,挺急的不能用的话得赶紧看新的/

  • 您好,
    ADC电路能达到的ENOB(Effective Number of Bits )与您的电路设计有很大关系,ADC输入信号和输入时钟信号的干净度对其性能也有很大影响
    您指的是补偿插入损耗吗,这个应该不是通过寄存器设置实现的,为更加有效地解决您的问题,我问一下更了解这款芯片的TI资深工程师,再为您解答
  • 关于7.5位有效位数,这是实际值,不是理论值。
    关于插入损耗补偿,这里的意思是随着输入信号的值越来越高,插入损耗会增加,这需要由设备使用者或设备的最终用户进行补偿。也就是说,产品设计者可能需要在射频信号链中使用额外的增益,或者在FPGA中使用一些数字补偿/校正,等等,或者两者的组合。