This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位工程师好!我在使用TMUX1109做ADC差分同步采样,现在出现了很严重的串扰问题,我软件是在每次通道切换完成后100us才开始采样的,但是每个通道的波形始终有串扰,而且非常严重,通道不切换采样就不会有串扰,麻烦帮我看下是不是硬件或者软件哪里有注意事项没考虑到。谢谢!
8308.TMUX1109.pdf
您好!
1、TMUX1109是用的差分输入,信号电平小于2V,频率只有几十Hz
2、因为我的是差分信号,所以再切换过程中没办法用仪器看,我是把ADC采集的实时显示出来的。
3、TMU1109我们用了4个通道,串扰是X通道的信号再切换后,其他通道会出现一样的信号,我把我ADC采集的波形贴上来,这个应该不是耦合,因为我TMUX1109内部不切换的话,通道就不会串扰。