ADS1298上电初始化,管脚复位脉冲后,发关闭连续读指令,获得ID成功后,对各个寄存器配置,然后发送开始指令,再发送连续读指令,这些都成功完成后,在连续读取数据时,SPI获得的数值全为0。此时用示波器测量管脚电压,发现SPI的时钟是正常的,但DOUT输出端始终是低电平,DRDY管脚工作正常,可以定时出现希望的负脉冲,说明此时芯片的基本功能是正常的。一旦出现此现象,只要不断电和复位就会一直持续下去。但这个现象发生非常偶然,并不是每次上电都出现,不出现时,所有功能都正常,可以正确采集到波形数据。重新上电后又不出现此现象了。所以请问,这是什么原因造成的?会是寄存器配置的问题造成这个现象的发生吗?第二个问题是:我用V导联作起搏检测,用最低的采样频率,使用的是外部硬件比较电路输出反馈回GPIO的方式。此时将CONFIG2寄存器中的斩波截止频率位WCT_CHOP设置为1,斩波频率恒定,请问这样配置会对采到的信号有什么影响吗?谢谢