我移植msp430的ecg算法,但是发现430的算法滤波算法是针对采样频率是500sps的。现在我不能达到这么高的采样频率,我将ads1292的采样频率设置为125sps 。所以我需要修改它的滤波系数。不知道有没有人能提供一份针对125sps的滤波系数?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好, 1292最高可以到8k的,500应该不是问题,如下:
额,500采样点是能达到。。。但是我是用cc2540通过蓝牙发到ios上的,关于它们的传输速率,一直不能满足我500sps的速率。所以没办法 只能降低采样率。
你可以参考ads1292的开发板来连接。。。TI有提供的。下面是链接