ADS8339的REFIN输入了4.096V,VA脚电源供电为5V,VBD脚电源供电为3.3V,然后测试发现输入0-2.048V的AD转换为0-0xFFFF,2.048-4.096V的AD转换值也是从0-0xFFFF,测试发现IN+输入0.44V的AD值读取为14000多点,IN+输入2.5V的AD值也为14000多点,IN-接地。现在不知道问题出在哪里,请TI的工程师帮忙回复下,之前看到别人的帖子也有这个问题,我想问下是哪里的问题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.