This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP130 芯片应用问题

1.视频输入板卡->FPGA->视频输出板(DP130)->4K显示器,画面显示正常;

2.视频输入板卡->FPGA->视频输出板(DP130)->分析仪报错 link failed;

3.视频输入板卡->FPGA->视频输出板(DP130)->视频输入板(ITE6563+ITE68051), 无法识别;

4.FPGA测试程序,固定输出->视频输出板(DP130)->视频输入板(ITE6563+ITE68051), 画面显示正常;

怀疑时AUX通道造成的影响,请问该怎么定位问题,下面时DP130应用原理图

  • 您好,
    感谢您对TI产品的关注!为更加有效地解决您的问题,我需要询问更了解这款芯片的TI资深工程师,再为您解答,一旦得到回复会立即回复给您。
  • 您好,感谢您的耐心
    1. 请将电容 C123 由1uF 改为 0.22uF
    2. 为什么使用 R73 和 R74? 是为了满足FPGA共模电压要求?
    3. 是否有DP AUX分析仪来捕捉每种情况下的DP链路训练?
    4. 是否也可以读取每种情况下的DP130 DPCD寄存器?
  • 1.电容C123已改为0.22uF

    2.R69、R70电阻已去掉

    3.视频输出板(DP130)->视频输入板(ITE6563+ITE68051),读取AUX 数据如下表

       a)不清楚什么情况下会触发不停的read edid;

       b)另外视频输出板FGPA是以配置的参数固定输出时序,不使用EDID数据,那DP130屏蔽read edid操作吗

    1 Set Power State: NORMAL (D0)
    7 [DP_I2C] Start reading EDID
    28 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    56 [DP_I2C] EDID Extension Block (1: CEA-861)
    58 [RX_CAP] Max_Link_Rate: HBR2 (5.4G)
    59 [RX_CAP] Max_Lane_Count: 4
    [RX_CAP] TPS3_SUPPORTED ; EN_FRAME_CAP
    60 Set Power State: DOWN (D3)
    62 [LINK_CONFIG] Link_Rate: HBR2 (5.4G)
    64 [LINK_CONFIG] Lane_Count: 4 ; No Enhanced_Frame_EN
    65 [RX_CAP] DP v1.4 ; No Downstream-Facing Port! ; Extended Receiver Capability field - Present
    71 [LINK_CONFIG] Lane_Count: 4
    72 Set Training Pattern: TPS1
    73 Link Training: Clock Recovery... done
    [SINK_STATUS] POST_LT_ADJ (LQA) done
    74 Set Training Pattern: TPS3
    75 Link Training: Done (HBR2 ; 4 lanes)
    77 Training Pattern: Disabled
    83 [DP_I2C] Start reading EDID
    104 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    110 [SINK_STATUS] Sink Count = 1 (CP_READY)
    Link Training: None
    117 [DP_I2C] Start reading EDID
    138 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    146 Set Power State: NORMAL (D0)
    156 [DP_I2C] Start reading EDID
    177 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    184 Set Power State: DOWN (D3)
    185 Set Power State: NORMAL (D0)
    195 [DP_I2C] Start reading EDID
    216 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    223 Set Power State: DOWN (D3)
    224 Set Power State: NORMAL (D0)
    234 [DP_I2C] Start reading EDID
    255 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    262 Set Power State: DOWN (D3)
    263 Set Power State: NORMAL (D0)
    273 [DP_I2C] Start reading EDID
    294 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    301 Set Power State: DOWN (D3)
    302 Set Power State: NORMAL (D0)
    312 [DP_I2C] Start reading EDID
    333 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    340 Set Power State: DOWN (D3)
    341 Set Power State: NORMAL (D0)
    351 [DP_I2C] Start reading EDID
    372 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    379 Set Power State: DOWN (D3)
    380 Set Power State: NORMAL (D0)
    390 [DP_I2C] Start reading EDID
    411 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    418 Set Power State: DOWN (D3)
    419 Set Power State: NORMAL (D0)
    429 [DP_I2C] Start reading EDID
    450 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    457 Set Power State: DOWN (D3)
    458 Set Power State: NORMAL (D0)
    468 [DP_I2C] Start reading EDID
    489 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    496 Set Power State: DOWN (D3)
    497 Set Power State: NORMAL (D0)
    507 [DP_I2C] Start reading EDID
    528 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    535 Set Power State: DOWN (D3)
    536 Set Power State: NORMAL (D0)
    546 [DP_I2C] Start reading EDID
    567 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    574 Set Power State: DOWN (D3)
    575 Set Power State: NORMAL (D0)
    585 [DP_I2C] Start reading EDID
    606 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    613 Set Power State: DOWN (D3)
    614 Set Power State: NORMAL (D0)
    624 [DP_I2C] Start reading EDID
    645 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    652 Set Power State: DOWN (D3)
    653 Set Power State: NORMAL (D0)
    663 [DP_I2C] Start reading EDID
    684 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    691 Set Power State: DOWN (D3)
    692 Set Power State: NORMAL (D0)
    702 [DP_I2C] Start reading EDID
    723 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    730 Set Power State: DOWN (D3)
    731 Set Power State: NORMAL (D0)
    741 [DP_I2C] Start reading EDID
    762 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    769 Set Power State: DOWN (D3)
    770 Set Power State: NORMAL (D0)
    780 [DP_I2C] Start reading EDID
    801 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    808 Set Power State: DOWN (D3)
    809 Set Power State: NORMAL (D0)
    819 [DP_I2C] Start reading EDID
    840 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    847 Set Power State: DOWN (D3)
    848 Set Power State: NORMAL (D0)
    858 [DP_I2C] Start reading EDID
    879 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    886 Set Power State: DOWN (D3)
    887 Set Power State: NORMAL (D0)
    897 [DP_I2C] Start reading EDID
    918 [DP_I2C] EDID Basic Block (KYS-9000P1_11)
    925 Set Power State: DOWN (D3)
    926 Set Power State: NORMAL (D0)
  • 您能拿一个万用表在交流耦合电容之前AUXP和AUXN上测量AUX 的共模电压吗?
    对于DP130,交流耦合电容前的共模电压需要在0到2V之间。如果共模电压在范围内,DP130将只通过AUX 通信量。
  • 测量电压0.02V左右
  • R71是不是没有焊接,您可以焊接上R71吗
    电路图中AUXP上是100k下拉、AUXN上是100k上拉,因此我预计AUXN上的电压大约为3V,您能再次检查AUXN共模电压测量值吗?
  • R71根据参考设计焊接了。
    AUXN电压2.8V
  • 请确保CAD_SNK是低电平。AUXP约为0V,AUXN约为3V,那么DP130应该通过AUX数据。
  • 上面已确认,下图是分析仪抓到的数据,请问Set power state: DOWN什么情况下会出现,这个command会导致重新training,这个命令会产生哪写影响

  • 我在E2E论坛咨询的您的问题,我看到您有同时发帖,现在E2E论坛的工程师已经回复,请继续跟进,由E2E论坛的工程师为您提供更好的支持:
    e2e.ti.com/.../3658241