This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2112数据手册的疑问咨询

Other Parts Discussed in Thread: FDC2112, FDC2112-Q1

FDC2112手册第17页,关于转换时间的描述,这一段是怎么得到1.8ms,3.2ms,0.75ms以及最终的16.75ms的?

能描述一下计算过程吗?

The deterministic conversion time of the FDC allows data polling at a fixed interval. For example, if the
programmed RCOUNT setting is 512 FREF cycles and SETTLECOUNT is 128 FREF cycles, then one conversion
takes 1.8ms (sensor-activation time) + 3.2ms (conversion time) + 0.75ms (channel-switch delay) = 16.75ms per
channel.

  • 另外,手册19页提到差分配置下,传感器电容的计算公式为CSECSOR = 1/(L*(2*PI*fSENSOR)^2)-C。

    但是手册没有给出单端配置下,传感器电容的计算公式。能否提供一下?

  • 您好,
    感谢您对TI产品的关注!
    单端配置的计算公式是和差分配置下使用一样的计算公式
    关于上述时间的计算我再确认一下
  • 你好!我用同一个电容(20pF),分别接成差分和单端模式进行测试,都采用差分的计算公式进行计算,结果差异很大。差分模式结果与20pF接近,单端模式结果只有11pF。在应用手册snoa952 <Ground Shifting in Capacitive Sensing Applications>里有提到另一个频率计算公式(第2页),看起来是单端的连接方式。麻烦确认一下,谢谢!

  • 这个数据手册里的计算是不对的,新的版本尚未发布,请参阅FDC2112-Q1 数据手册里16页的计算

    应用手册snoa952讲的是,电容测量值都会受到设备附近是否有接地物体的影响,不同的地面配置对测量系统的影响
    差分和单端接法其寄生电容应该是不一样的,您在不接电容传感器时,测量寄生电容了吗
    在测量电容传感器后,其测量值要减去这个寄生电容值