This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7720的时间分辨率有多少?

Other Parts Discussed in Thread: TMS320F28379D, ISO7720

TI你好,我设计了一个电源产品,由于占空比很低,需要隔离的高精度PWM信号,我的方案如下:

1)采用TMS320F28379D的HRPWM模块,输出高精度PWM。PWM的频率为500kHz(2us周期),HRPWM的时间分辨率是0.18ns,理论上HRPWM的精度为0.0095%。

2)HRPWM输出通过RC滤波接到ISO7720的输入,R=10Ω,C=22pF。

3)ISO7720输出接功率芯片的驱动,功率芯片为CSD97395。

4)PWM的占空比正弦变化,占空比幅值为0.01,频率为50Hz。

问题:实验中发现,CSD97395的输出电压波形呈现出明显的台阶状,反推出来驱动信号的时间分辨率只有10ns左右。

ISO7720的最大传输速率为100M,是否可以推测上面问题产生的原因为ISO7720的时间分辨率不够?