This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS9110EVM

Other Parts Discussed in Thread: ADS9110EVM-PDK

我想问一下ADS9110EVM板上的BR24G32FVT之中是否存储了固件?还是PHI控制部分只是对其进行写操作?

  • 您好,EVM板子上的EEPROM应该是已经将固件加载进去了,EVMuser's guide中介绍:The SD card and EEPROM come pre-programmed with the information required to configure and initialize the ADS9110EVM-PDK platform. Once the hardware is initialized, the SD card and EEPROM
    are no longer used. EEPROM和SD card是来预先编程与配置和初始化ADS9110EVM板的.
    如果EEPROM固件没有加载进去的话,当打开EVM GUI使用PHI进行操作和控制时,应该会有提示或者报错之类的信息。
  • 所以预编程的固件是没有的吗?想请问下有没有预编程的固件可以提供
  • 您好,很抱歉,我们不提供关于这个EVM 固件的任何细节信息呢。 因为它是对于很多EVM板都是适用的, 作为code example并不是很有用。 所以给您带来不便非常抱歉。