This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867E的SGMII接口使用。



使用FPGA的LVDS_serdes模式驱动这个PHY芯片,但是可以不使用PHY芯片上自带的SGMII_SCO(625MHz)的时钟吗?现在我用的是CYCLONE 10GX的FPGA,需要在一个BANK上驱动两个以太网SGMII接口。

  • 您好, 这个是6 wire SGMII interface接口的差分时钟输出引脚, 是需要和MAC连接的,用于MAC无法恢复时钟,需要外部给MAC提供时钟.
    如果是4 wire SGMII接口的话,这个时钟SGMII_COP/CON就不需要使用.
  • 也就是说,我这边可以不使用这个时钟,因为我看到一个88E1111-B2-NDC2C000的PHY设计的SGMII接口也是这个时钟没有使用,只用了输入和输出差分线,这个使用内部的lvds_serdes(带DPA功能)的IP核是不是就可以了,还是说需要用lvds_serdes(带cdr功能)的IP核才可以?