Hi TI Team,
Thanks for your continuous supporting for my queries.
I am using ADS8671 and F28335 in my design.
I write the read_HWORD instruction to ADS8671 through F28335.The command is 0xC802 and 0x0000 which is used to read DEVICE_ID_REG. In the data-sheet, the result is 0x0000 0000.But the actual return is 0xA420 000E.
In addition ,the device always works in default mode. It cant respond to the command I typed correctly. So I can't configure his input range and the output content.
Thanks and Regards,
tengfei_cui