This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8760: DAC8760在电流输出时如何禁用VOUT

Part Number: DAC8760


你好,请问DAC8760在切换输出为电流输出时,VOUT引脚一直会有一个变化的电压,在电流输出时我如何禁用VOUT呢?

  • 您好,

    将 Configuration寄存器的[10:7]位配置为0 ,Control寄存器的 RANGE bits配置输出范围,您是这样配置的吗

  • 是的,下面是我初始化的程序;

    int main(void)
    {
    init_readConfig();
    system_init();
    //DAC8760_Setup((DAC8760_RANGE_0V_10V + DAC8760_OUTEN), 0, 0, 0);
    //DAC8760_SetOutValue(0x0);
    SysCtlDelay(10000);
    switch (DA_Setup_user[1])
    {
    case 0:// -10~+10V
    DAC8760_Setup((DAC8760_RANGE_M10V_P10V + DAC8760_OUTEN), 0, 0, 0);
    DAC8760_SetOutValue(32767);// Set DAC8760 output value to 0V
    break;
    case 1:// 0~10V
    DAC8760_Setup((DAC8760_RANGE_0V_10V + DAC8760_OUTEN), 0, 0, 0);
    DAC8760_SetOutValue(0); // Set DAC8760 output value to 0V
    break;
    case 2:// 0~5V
    DAC8760_Setup((DAC8760_RANGE_0V_5V + DAC8760_OUTEN), 0, 0, 0);
    DAC8760_SetOutValue(0); // Set DAC8760 output value to 0V
    break;
    case 3:// 0~20mA
    DAC8760_Setup((DAC8760_RANGE_0MA_20MA + DAC8760_OUTEN), 0, 0, 0);
    DAC8760_SetOutValue(0); // Set DAC8760 output value to 0V
    break;
    case 4:// -5~+5V
    DAC8760_Setup((DAC8760_RANGE_M5V_P5V + DAC8760_OUTEN), 0, 0, 0);
    DAC8760_SetOutValue(32767);// Set DAC8760 output value to 0V
    break;
    case 5:// 4~20mA
    DAC8760_Setup((DAC8760_RANGE_4MA_20MA + DAC8760_OUTEN), 0, 0, 0);
    DAC8760_SetOutValue(0); // Set DAC8760 output value to 0V
    break;
    default:
    DAC8760_Setup((DAC8760_RANGE_M10V_P10V + DAC8760_OUTEN), 0, 0, 0);
    DAC8760_SetOutValue(32767);// Set DAC8760 output value to 0V
    break;
    }

    }

    void DAC8760_Setup (uint16_t controlReg, uint16_t configurationReg, uint16_t gainCalReg, uint16_t zeroCalReg)
    {
    DAC8760_SPISetupMaster();
    DAC8760_Reset();
    DAC8760_Nop();
    DAC8760_WriteReg (controlReg, DAC8760_WRITE_CONTROL_REGISTER);
    DAC8760_WriteReg (configurationReg, DAC8760_WRITE_CONFIGURATION_REGISTER);
    DAC8760_WriteReg (gainCalReg, DAC8760_WRITE_GAIN_CALIBRATION_REGISTER);
    DAC8760_WriteReg (zeroCalReg, DAC8760_WRITE_ZERO_CALIBRATION_REGISTER);

    }

  • 抱歉,我这里无法验证您的程序,您可以把您配置的寄存器值读出来告诉我吗?我看一下Configuration和Control寄存器您是写入的是什么