This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS124S08: AD芯片的多通道配置问题

Part Number: ADS124S08


大家好,

      最近我正在使用ADS124S08,计划使用两通道同时采集数据,采集频率不同,分别是10SPS和200SPS。我想请问的是:因为输出数据并不含有通道信息,所以取数据只能取当前配置通道的信息么?我需要自己在主MCU中利用定时器定时去配置02、03和04寄存器然后发送采集命令采集数据么?有没有更简便的采集方案?

  • 您好, ADS124S08虽然是多通道输入,但是它内部只集成了一个ADC,具体选择哪个通道采集数据,是通过输入前端的多路选择器进行配置.

    寄存器02h为Input MUX的配置地址,配置哪个通道导通,那么ADC就对哪个通道的信号进行采集. 所以输出的数据即为您配置的这个通道.