This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298: 肢体导联脱落会影响胸导联的数据为直线的问题是否有解决办法?

Part Number: ADS1298


 如图所示,我参考ADS1298的评估板的方式按此顺序连接的各个导联线位置。在实际测试使用中发现,如果各个导联正常连接人体,各通道的信号基本是正常的,基线大概在几十mV上下。但是,在有些人体佩戴时,当肢体导联LL,LA,RA,有一个脱落后,胸导V1V2V3V4V5V6上的信号都会变成直线,从读出的数据推断好像是胸导的数据超出了测量范围;但有的人体佩戴时,如果肢体导联脱落,胸导各通道也会有心电数据波形,但此时各导联的基线很高达到300多mV。根据WCT的原理,胸导的负端输入为三个肢体导联的平均值,是否是因为肢体导联脱落造成平均值过大,使得V导转换超出了测量范围所导致的?我采用的是低功耗模式3V供电参考电压为2.4V,默认是使用6倍放大。请问是否有什么办法改善一下,在肢体导联脱落后胸导也能输出波形。谢谢

  • 您好,

    如您所说,WCT是三个肢体导联的平均值,而胸导联是以WCT电压作为其基准电压测量的,因此,如果有一个肢体导联(RA、LA、LL)脱落,那么WCT值也就不准确了,即使胸导联有心电数据波形,因为它是在WCT基础上测量的,那么胸导联测得心电波形也是不准确的,后期再怎么处理也是不准确的,也就没有测量的意义了