This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ3200: 可以不使能sysref校准吗?

Part Number: ADC12DJ3200


校准是为了满足建立保持时间,那可以选择直接用sysref可以吗?

还有就是,可以正常编程完ADC之后我再发sysref吗?

  • 您好, 在8.3部分的初始化步骤完整之后,即第14步之后就可以使能SYSREF校准了。

    如果您是使用多个ADC12DJ3200,需要保持同步或者确定性延迟的话,需要enable SYSREF校准, 如果只有一片ADC使用,那么使能JESD接口(JESD_EN=1),自动校准就可以了。

    8.3 Initialization Set Up

    The device and JESD204 interface require a specific startup and alignment sequence. The general order of that sequence is listed in the following steps.

    1. Power-up or reset the device.
    2. Apply a stable device CLK signal at the desired frequency.
    3. Program JESD_EN = 0 to stop the JESD204B state machine and allow setting changes.
    4. Program CAL_EN = 0 to stop the calibration state machine and allow setting changes.
    5. Program the desired JMODE.
    6. Program the desired KM1 value. KM1 = K-1.
    7. Program SYNC_SEL as needed. Choose SYNCSE or timestamp differential inputs.
    8. Configure device calibration settings as desired. Select foreground or background calibration modes and offset calibration as needed.
    9. Program CAL_EN = 1 to enable the calibration state machine.
    10. Enable overrange via OVR_EN and adjust settings if desired.
    11. Program JESD_EN = 1 to re-start the JESD204B state machine and allow the link to restart.
    12. The JESD204B interface operates in response to the applied SYNC signal from the receiver.
    13. Program CAL_SOFT_TRIG = 0.
    14. Program CAL_SOFT_TRIG = 1 to initiate a calibration.