ADS1284在使用过程中,是否涉及到不同增益的情况下阻抗匹配不一致的问题,就是说,连接不同传感器,输入在0dB和24dB增益的情况下,表现一致,只有在12dB表现不一致,这是怎么回事呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
传感器输出阻抗2K。我们有3种电路板,只是在传感器入口处设计不一致,其余包括和AD有关的电路、程序均是一致的。3种电路板同源测试,记录一定时间的采集幅值,当电路设置在0dB、24dB时候,幅值完全一致,当设置在12dB的情况下,3种电路幅值只有在较高幅度的情况下,出现不一致,幅度较低的情况完全一致。当把传感器换成信号源,使用较高幅值的正弦波,12dB的情况下,3种电路幅值又一致了,不知道为什么会出现这种现象。我们传感器为动圈式检波器,问题1:均使用检波器时,为什么12dB在幅值较高的地方出现差异,幅值低的情况下一致。问题2:使用信号源上述现象消失,检波器和信号源有什么区别吗,会引发上述现象