Hi team
Good day!
客户有个问题需要咨询:
ADS7495 33页低通滤波器的设计问题,ADC前面的低通滤波器是为了滤除什么噪声,我根据公式计算求出低通滤波器的截止频率特别大,我知道他是要滤除什么波,为什么要设计那么大。
找了好多TI相关的信息,我发现通过计算得到的频率都很大,为什么要把截止频率设置这么大,是为了滤除什么噪声么?
Regards
Aosker
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team
Good day!
客户有个问题需要咨询:
ADS7495 33页低通滤波器的设计问题,ADC前面的低通滤波器是为了滤除什么噪声,我根据公式计算求出低通滤波器的截止频率特别大,我知道他是要滤除什么波,为什么要设计那么大。
找了好多TI相关的信息,我发现通过计算得到的频率都很大,为什么要把截止频率设置这么大,是为了滤除什么噪声么?
Regards
Aosker
感谢回复
客户方回复:ADS内部输入电容会在采样时会产生一个干扰。我们设计低通不是为了滤除干扰吗,干扰频率是多少?图86设计的低通滤波器截止频率根据公式计算为六千五百多万Hz,为什么需要这么大。
因为这个干扰是在开始采样时产生的,这个干扰频率应该与采样频率有关,外部滤波器必须确保输入能够在所选采样时间内达到所需的精确度。根据下面datasheet截图公式(1),是这个采样时间与滤波器的时间常数的一个关系式。可以看出采样频率越高采样时间越小,滤波器的时间常数越小,滤波器的截止频率越高。滤波器的截止频率计算公式为公式(3)
公式(1)和(2)都是对时间常数的计算,不能计算截止频率,我很疑惑您是怎样用公式(1)和(2)计算截止频率的;
我的理解是 公式(1)是输入信号在所选采样时间内达到稳定 需要的时间;
公式(2)是滤波器的时间常数,通俗来讲,这个时间常数越大,滤除干扰的时间就会越长,因此需要满足公式(1)的要求,即滤波器的时间常数最大只能为公式(1)等号右边的时间;这样滤波器的时间常数定了,截止频率也就定了即公式(3)
公式3里不是有个tAU吗。公式1、2都给出了时间常数的计算。您是用公式1里的tAU代入到公式3求得的截止频率。我现在疑惑的是为什么不能用公式2里的tAU代入到公式3呢。我看了很多资料说ADS前面要有一个抗混叠滤波器。它是一个低通滤波器,低通滤波器的截止频率不是1/2πRC吗,在ADS7945的p34中说明了对应的图中R、C的值
第1个公式与第2个公式所表示的都是时间常数,在图中是一样的也没做区分,很让人疑惑。公式1只需要知道采样率和分辨率就可以了,这个一阶RC的设计有什么关联呢。您的意思是说公式2算出的时间虽然比公式1大,但这个时间不会超过公式1计算的时间。所以公式1的时间才是真正的滤波时间常数吗???所以公式3里的滤波时间常数是用公式1的而不是公式2的
还有您说不知道怎么用公式1、2算截止频率的。公式3算的带宽不就是RC低通滤波器的截止频率吗。我现在的疑惑是tAU代入公式1还是公式2的。我认为应该是公式2的,您认为是公式1的
这样说吧,现在是不是要设计一个滤波器,滤去采样时产生的干扰?这个滤波器需要确定其截止频率是多少,其截止频率就是1/(2πRC),因为这个滤波器还没设计出来,它的R和C参数都是不知道的,那么怎样确定它的参数呢?不管怎样这个滤波器的参数不能影响电路的精度,也就是需要满足采样时间与滤波器时间常数的关系式公式(1)。那么好了,由公式(1)确定了时间常数RC,代入公式(3)就是截止频率了,同时也可以确定R和C的值了,滤波器也就设计出来了